Incosinstent pinout description on MC56F844XX 48LQFP package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Incosinstent pinout description on MC56F844XX 48LQFP package

449 Views
mansski
Contributor I

Hi, I am planning to use MC56F84451 and I have a problem figuring what are the functions of pins 36 and 38. The manual describes no function for pin 36 and has contradicting functions described for pin 38. I am using the document MC56F844XX.pdf (Rev. 3, 06/2014) looking at the table on page 24 and 25 where there is twice a description for pin 38 - first as GPIOE3 and then as GPIOF1 ?! (the 48 LQFP), and no description whatsoever for pin 36.

Labels (1)
0 Kudos
1 Reply

290 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Stanko,

Pls refer to section 8.3 Signal Multiplexing and Pin Assignments in MC56F844xxRM.pdf, I copy the part here.

This is the pin assignment:

for 48 pins MC56F84451:

pin36:GPIOE3 PWMA_1A

pin38:GPIOF1 CLKO1 XB_IN7 CMPD_O

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 Kudos