StoredReference of ADC calibration of ZVC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

StoredReference of ADC calibration of ZVC

644 Views
zhangcindy
NXP Employee
NXP Employee

In Flash IFR Mapping(table 1-16 of MC9S12ZVCRMV1_Rev1.5), StoredReference of ADC calibration is from bit 15-5, But I had read 0x1F C040 my evk(Marking is P912ZVCA19A), it is 0x03dd and seems it is bit 11-0.  Please confirm if it is correct in RM.

Labels (1)
0 Kudos
1 Reply

379 Views
RadekS
NXP Employee
NXP Employee

Hi Xin,

You are right, it seems that there is an error in S12ZVC RM documentation (Rev1.5) and stored ADC reference is right aligned instead of documented left aligned.

I already reported it.

Thank you for notification.

 

BTW: The simple example code how to use ADC calibration with these values is located at:

https://community.nxp.com/docs/DOC-332475

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos