#中国用户论坛#申请LPCXpresso54608,基于LPC54608的串口屏设计

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

#中国用户论坛#申请LPCXpresso54608,基于LPC54608的串口屏设计

1,610 Views
gaoxiaojun1
Contributor I

        近期了解到NXP推出LPC5460x系列产品,尤其是设计了LPCXpresso54608开发板,功能非常强大,方便开发和初期性能测试。之前用过LPC1788,与LPC1788相比,LPC54608在各个方面都在强很多,比如主频从120M提升到了180M,SRAM由96KB提升到了200KB,USB由Full Speed提升最高到High Speed,ADC由400KHz提升到了5M采样率,其它还有增加了AES和SHA等等,其它还有很多性能都全面超越LPC1788系列。
      将来在USB大数据量传输、ADC 12位精度能满足要求的应用中(就目前来看5M采样率足够,直接省掉外部ADC)、数据安全要求的场合,LPC5460x都非常适合。

        在此之前,设计过基于LPC1788FBD144 + SDRAM + TFT LCD的工业用串口LCD显示屏,LCD分辨率1027 x 768。LPC5460x虽然在LCD控制器最大分辨率仍然为1024x768,但是满足一般14寸以下的中小型LCD应用绰绰有余,而整体性能却比LPC1788提高了近一倍,在做LCD显示的同时,可以兼做其它外设控制。

        在使用LPC1788前,一直是在使用ST的STM32F10X系列产品,由于产品需要而ST公司的产品无法满足要求。于是考查了几个厂家的ARM MCU产品,最后在NXP与nuvoton之间做取舍。

        nuvoton产品在MCU内嵌大容量SDRAM,但是产品温度等级只能达到低温-20℃,而要达到-40℃的话,只能通过整机成品做低温性能筛选;

        NXP的LPC1788虽然内部没有大容量SDRAM,但是由于温度等级为-40℃,外挂SDRAM选型灵活容量也容易控制,也考虑到同一系列产品将来可能会有升级。最后确定使用LPC1788方案来实现,最终产品方案完美实现,目前经过两年多的持续供货,工业客户反馈良好。

      

      错过了第一季的LPC54608开发板免费申请活动,希望这次能通过申请。

     

      NXP社区 论坛 - 手机版 - Powered by Discuz!  活动价购买了LPC824 Lite开发板和LPC824 Breakout开发板,并对性能和几乎全部的外设做了全方位测试学习,基于这两款开发板参加了eeboard的活动。活动发贴合集见,【赚周年币】技术帖Week3-Day3——LPC824 学习合集
http://www.eeboard.com/bbs/forum.php?mod=viewthread&tid=63202&fromuid=17147

Labels (3)
0 Kudos
1 Reply

1,258 Views
joezhou-mcu
Contributor III

谢谢你对LPC1788的应用分享。-40C到105C是LPC工业级产品的标配。

0 Kudos