Supported GPS module for iMX6Q sabre AI board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Supported GPS module for iMX6Q sabre AI board.

663 Views
vishalgautam
Contributor II

Hi Experts,

We are working on iMX6Q sabre AI board. As per the attached Android release notes for i.MX AndroidTM M6.0.1_1.0.0 mentions that for this board GPS connectivity is not applicable but in the attached board schematic diagram interface for GPS module is mentioned.

Our requirement is to use GPS with this board. Please suggest which GPS module (vendor & module part no.) works with iMX6Q sabre AI board & what software changes are required to get GPS module up & running on this board.

Below is the software stack (BSP) I am using

OS:- Android Marshmallow 6.0.1

Kernel:- 3.14.52

U-boot:- 2015.04

Waiting for your reply.

Thanks & Regards,

Vishal Gautam

0 Kudos
1 Reply

383 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vishal

board hardware supports gps uart connection, however no drivers are provided

according to Release Notes. Please check

https://community.nxp.com/message/307613 

GpsStatus.NmeaListener | Android Developers 

android - How to read GPS data and accelerometer data in one activity - Stack Overflow 

geolocation - How do I get the current GPS location programmatically in Android? - Stack Overflow 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos