poweroff mx6 in u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

poweroff mx6 in u-boot

1,481 Views
GregT
Contributor III

Does anyone know of a function in u-boot that can be called to power off the mx6 processor similar to the poweroff available in Linux?  Thanks.

Labels (2)
0 Kudos
3 Replies

785 Views
BiyongSUN
NXP Employee
NXP Employee

Set TOP field in SNVS_LP Control (LPCR), which will trigger i.MX6 PMIC_ON_REQ with the Dump PMIC enabled.

Untitled.png

785 Views
Yuri
NXP Employee
NXP Employee

Hello,

  If board hardware allows it - it is possible to use i.MX6 PMIC_ON_REQ signal

to switch off external PMIC.

 

How to control the PMIC_ON_REQ pin by SW without ON/OFF pin for i.MX6 

Regards,

Yuri.

785 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi GregT

For proper answer and discussion, Please check:

https://community.nxp.com/thread/307212 

Regards