I purchased a FRDM-K64F. I plugged it into a Windows 10 PC. After plugging the K64 board into the PC, I tried to install the mbed serial driver (mbedWinSerial_16466.exe). This application does not install and I get an error "mbed x64. Could not install the driver". After installing the serial driver, I tried to get the board to come up in boot-loader mode. The board doesn't come up in Bootloader" mode either. When the board is plugged in Windows pops up a message that says "USB device is not recognized".
A couple of questions
1) Should the mbed or openSDA serial driver to be installed for the FRDM-K64F?
2) After further reading I see a warning not to install the K64 with openSDA2 into a windows 10 PC. IS this the case
Has the board become corrupt?
Any help would be appreciated.
Malcolm
Solved! Go to Solution.
Thanks to both of you for your .replies. It is now working!!
Malcolm
Hi Malcolm,
To provide the fastest possible support I want to point you to a similar question which has been answered on our NXP community. Please refer to https://community.nxp.com/docs/DOC-330935 to view the details.
To help NXP improve the technical support via communities please rate the answer given in the referred thread.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Malcolm
You need to get the latest P&E driver and/or the latest mdeb one (P&E will allow debugging) since the version that was pre-installed was probably one that is not compatible with Win 10.
To install you may need to find a Win 7 PC though (or disable the way that Win 10, or Win 8 works with external drives - there are some guides to doing it if you search the Internet).
Your board should be OK once you have been able to install a suitable driver version.
Regards
Mark