I want to create a project with the following :
Board - FRDMK66F
RTOS - MQX
Interfaces - UART, SPI, I2C, SDIO
Additional features - RTCS, USB, LWIP
Toolchain - KDS
Please help me to do this. It will be very helpful, if you can share the document which contains the procedure followed.
I would like to suggest you read the following document for creating a MQX project with KDS.
How To: Create a New MQX RTOS for KSDK Project in KDS
If you use IAR, please refer to the following link
https://community.nxp.com/docs/DOC-105525
You also can refer to the MQX demo project based on K66 in ksdk.
C:\Freescale\KSDK_1.3.0\examples\frdmk66f\demo_apps\i2c_rtos\i2c_rtos_mqx\kds
Have a great day,
Daniel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------