Library for CLRC663 and Kinetis (KDS).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Library for CLRC663 and Kinetis (KDS).

838 Views
cerma
Contributor IV

Hello everybody,

I am using FrontEnd CLRC663 and Kinetis MK61. I would like to start using library NFCReaderLibraryForCLEV663B-04.030.00.011627. BAL layer is written for processors LPC. Are you going to write it for Kinetis and project for KDS as well? If so when it will be released? If not, is there any list of components and their settings in BAL layer? For example: 4 timers are used. First is set to ...microseconds, etc. It would be easier than pull this things out of code for LPC.

Thank you.

Jaroslav

Tags (5)
0 Kudos
1 Reply

494 Views
isaacavila
NXP Employee
NXP Employee

Hello,

NFC library was planned to be migrated to Kinetis family by the end of december (https://community.nxp.com/thread/431919 ).

I will let you know as soon as this release is available.

Regards,

Isaac

0 Kudos