Hi,
I am trying to enable UART interrupt for Imx6q. I have initialized the GIC, UART, set the interrupt state, registered the handler, and enabled the interrupt. But after enabling the interrupt, the normal execution halts. On further analysis it was seen that the execution halts when i set the "GICD_ISENABLERn" register of the GIC. But, even if the normal execution halts, it enters the "IRQ_HLDR" for once and executes till the end of the handler.
Then, i tried initializing the gic only after the interrupt has been enabled. In that case the program does not halt when i set the "GICD_ISENABLERn" register, but when i set the "gicd->CTLR" for enable forwarding the secure and non-secure interrupt. Even then, the "IRQ_HLDR" executes once as before. What might be the problem? am i forgetting some initialization steps? I have attached my main,gic and interrupt files. Please do ask if need anything else. Please help..
Original Attachment has been moved to: vectors.S.zip
Original Attachment has been moved to: startup.S.zip
Original Attachment has been moved to: main.c.zip
Original Attachment has been moved to: gic.c.zip
Original Attachment has been moved to: gic.h.zip
Original Attachment has been moved to: interrupt.c.zip
Original Attachment has been moved to: interrupt.h.zip
Solved! Go to Solution.
Hi ajmalali
please look at attached sdk example with description in pdf file
Chapter 4 Configuring the GIC Driver. For obtaining full sdk one
can create service request.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ajmalali
please look at attached sdk example with description in pdf file
Chapter 4 Configuring the GIC Driver. For obtaining full sdk one
can create service request.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ~Igor,
Thanks for the reply.
I have referred "1.1.0_iMX6_Platform_SDK" for writing the above. The problem occure when i set the "GICD_ISENABLERn" or "gicd->CTLR" as done in the sdk. what might be the problem ?
regards,
Ajmal
Hi Ajmal
please check uboot gpio interrupt example, it may be modified for uart
Best regards
igor