MFG Download fail on Sabresd Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG Download fail on Sabresd Board

1,687 Views
david5icp
Contributor III

Hi All,

  I bought a new sabresd board for test. The board can boot linux form SD card (on SD3 Slot). The borad should be fine.

Now i try to use MFG tool to download Android Image to eMMC, But always fail. the log as below:

----------------------------------------------------------------------------------------------------------------------------------------

U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g53e6f33 (Nov 01 2015 - 13:59:48)

CPU:   Freescale i.MX6QP rev1.0 at 792 MHz
CPU:   Temperature 40 C
Reset cause: POR
Board: MX6-SabreSD
I2C:   ready
DRAM:  1 GiB
PMIC:  PFUZE100 ID=0x10
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc1 is current device
Net:   FEC [PRIME]
Boot from USB for mfgtools
Use default environment for                              mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot:  0
Kernel image @ 0x12000000 [ 0x000000 - 0x521128 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
   Image Name:   fsl-image-mfgtool-initramfs-imx6
   Image Type:   ARM Linux RAMDisk Image (gzip compressed)
   Data Size:    7487205 Bytes = 7.1 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
   Booting using the fdt blob at 0x18000000
   Using Device Tree in place at 18000000, end 1800d77d
switch to ldo_bypass mode!

-------------------------------------------------------------------------------------------------

Tools and Image are download form official web site:

 MFG tool version : IMX6_L5.1_2.1.0_MFG_TOOL.

 Android Image : IMX6_L5.1_2.1.0_AND_DEMO_SD_BS.tar.gz

 SW6 setting (1-8): 0000-1100

I Think the tools and firmware should be fine, does the borad has problem ?

Thanks!

BR.

David Wu

Labels (2)
0 Kudos
4 Replies

1,387 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

please check attached L5.1_2.1.0 Release Notes, seems

i.MX6QP sabresd support was added starting from M6.0.1_1.0.0,

please use mfg tools mfgtool2-android-mx6qp-sabresd-emmc.vbs

script for programming.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,387 Views
david5icp
Contributor III

Hi Igor,

 I had try both "mfgtool2-android-mx6q-sabresd-emmc.vbs" and "mfgtool2-android-mx6q-sabresd-sd.vbs",  but same results..

BR.

David Wu

0 Kudos

1,387 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

have you tried M6.0.1_1.0.0

~igor

0 Kudos

1,387 Views
david5icp
Contributor III

Hi Igor,

 Yes, I had try Androin 6.0 this morning, still same... log as below:

-----------------------------------------------------------------------------------------

U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g53e6f33 (Nov 01 2015 - 13:59:48)

CPU:   Freescale i.MX6QP rev1.0 at 792 MHz
CPU:   Temperature 37 C
Reset cause: POR
Board: MX6-SabreSD
I2C:   ready
DRAM:  1 GiB
PMIC:  PFUZE100 ID=0x10
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc1 is current device
Net:   FEC [PRIME]
Boot from USB for mfgtools
Use default environment for                              mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot:  0
Kernel image @ 0x12000000 [ 0x000000 - 0x521128 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
   Image Name:   fsl-image-mfgtool-initramfs-imx6
   Image Type:   ARM Linux RAMDisk Image (gzip compressed)
   Data Size:    7487205 Bytes = 7.1 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
   Booting using the fdt blob at 0x18000000
   Using Device Tree in place at 18000000, end 1800d77d
switch to ldo_bypass mode!

-----------------------------------------------------------------------------------------

BR.

David Wu

0 Kudos