i use the RTL8188 CUS usb wifi .
i can creat the AP without Wireless password by hostapd.
the hostapd.conf is:
interface=wlan0
driver=nl80211
ssid=ArmCat
hw_mode=g
channel=8
macaddr_acl=0
ignore_broadcast_ssid=0
it's work well.
but i want to add a password.and add this :
auth_algs=1
wpa=1
wpa_passphrase=12345678
wpa_key_mgmt=WPA-PSK
wpa_pairwise=TKIP CCMP
rsn_pairwise=CCMP
when i run the hostapd.
the log is:
rtl8192cu: MAC auto ON okay!
rtl8192cu: Tx queue select: 0x05
IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
Failed to update rate sets in kernel module
Using interface wlan0 with hwaddr 00:1d:43:a0:06:dc and ssid 'ArmCat'
random: Only 11/20 bytes of strong random data available from /dev/random
random: Not enough entropy pool available for secure operations
WPA: Not enough entropy in random pool for secure operations - update keys later when the first station connects
IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
i can't connet the AP by the password and warned wrong password.
I tried the following method:
mv /dev/random /dev/randombak
ln -s /dev/urandom /dev/random
the log :
rtl8192cu: MAC auto ON okay!
rtl8192cu: Tx queue select: 0x05
IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
Failed to update rate sets in kernel module
Using interface wlan0 with hwaddr 00:1d:43:a0:06:dc and ssid 'ArmCat'
IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
The same situation. warned wrong password.
why and how to solve this problem?
Board: MX6UL 14x14 EVK
Linux version 3.14.52-1.1.0_ga+g5f6f0a5
thanks!
Hello,
The following may help.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------