I.MX6UL can not start UBOOT from eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6UL can not start UBOOT from eMMC

4,121 Views
andyyang730
Contributor I

Dear Support

 we are trying to port u-boot into our own board,  the emmc and DDR part as below 

 eMMC:MTFC8GACAAAM-1M 

 DDR:MT41K256M16HA-125

DDR had passed stress test and we set the .cfg file using the test data. in MFG , we can download the uboot in to EMMC, the MFG return Done in the GUI.

then we set the chip start from emmc as the fuse map. after start up there is nothing print out from uart 1 , and after few seconds ,the chip will get into download  mode automatically.

Could you kindly help to give some suggestion.

thanks.

Labels (1)
0 Kudos
11 Replies

2,209 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

one can attach jtag and check registers SRC_SBMR1,2 for

correct boot settings, also please check emmc signals with

oscilloscope.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

2,209 Views
andyyang730
Contributor I

Dear Igor

thanks for your quickly reply

i test the register which you mentioned the result as below.

SRC_SBMR1(0x020d8004) = 0x0000c860
SRC_SBMR2(0x020d801c) = 0x02000001

pastedImage_3.png

and we try to catch the signal for CMD and CLK on EMMC ,we think that is right , there is a lot of signal when the board start up ..

below is our DDR info tested by test tool.

pastedImage_2.png

and below is the log info for download(i bypass to burn the rootfs due to that spend a lot of time ,and if i download rootfs into emmc ,that is the same).

CPU:   Freescale i.MX6UL rev1.1 at 396 MHz
CPU:   Temperature 55 C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C:   ready
DRAM:  512 MiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment

Display: TFT43AB (480x272)
Video: 480x272x24
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc1(part 0) is current device
Net:   Phy 1 not found
PHY reset timed out
FEC1
Error: FEC1 address not set.

Boot from USB for mfgtools
Use default environment for                              mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot:  0
Kernel image @ 0x80800000 [ 0x000000 - 0x557060 ]
## Loading init Ramdisk from Legacy Image at 83800000 ...
   Image Name:   fsl-image-mfgtool-initramfs-imx6
   Image Type:   ARM Linux RAMDisk Image (gzip compressed)
   Data Size:    7565342 Bytes = 7.2 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 83000000
   Booting using the fdt blob at 0x83000000
   Using Device Tree in place at 83000000, end 8300b8e9
Modify /soc/aips-bus@02000000/bee@02044000:status disabled
ft_system_setup for mx6

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.1.15+ (root@baite-B85M-D3V-A) (gcc version 4.8.3 20140320 (prerelease) (Sourcery CodeBench Lite 2014.05-29) ) #1 SMP PREEMPT Thu Oct 20 20:43:08 CST 2016
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board
Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB
Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @8bb32000 s16768 r8192 d24192 u49152
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= clk_ignore_unused
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 173464K/524288K available (6899K kernel code, 319K rwdata, 2348K rodata, 388K init, 423K bss, 23144K reserved, 327680K cma-reserved, 0K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0xa0800000 - 0xff000000   (1512 MB)
    lowmem  : 0x80000000 - 0xa0000000   ( 512 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .text : 0x80008000 - 0x809100f4   (9249 kB)
      .init : 0x80911000 - 0x80972000   ( 388 kB)
      .data : 0x80972000 - 0x809c1fc0   ( 320 kB)
       .bss : 0x809c4000 - 0x80a2df70   ( 424 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
        Additional per-CPU info printed with stalls.
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
mxc_clocksource_init 24000000
Switching to timer-based delay loop, resolution 41ns
sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80008280 - 0x800082f0
Brought up 1 CPUs
SMP: Total of 1 processors activated (48.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
device-tree: Duplicate name in lcdif@021c8000, renamed to "display#1"
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
mxs-dma 1804000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7392K (83800000 - 83f38000)
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
21c8000.lcdif supply lcd not found, using dummy regulator
mxsfb 21c8000.lcdif: failed to find mxc display driver
Console: switching to colour frame buffer device 60x34
mxsfb 21c8000.lcdif: initialized
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 19, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 235, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
fsl-quadspi 21e0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff
fsl-quadspi 21e0000.qspi: Freescale QuadSPI probe failed
20b4000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 20b4000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 20b4000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 6a:0a:da:0c:06:95
libphy: fec_enet_mii_bus: probed
fec 20b4000.ethernet eth0: registered PHC device 0
2188000.ethernet supply phy not found, using dummy regulator
pps pps1: new PPS source ptp1
fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 9a:35:6d:a8:b5:88
fec 2188000.ethernet eth1: registered PHC device 1
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184000.usb supply vbus not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
LUN: removable read only file: /fat
Number of LUNs=1
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
mousedev: PS/2 mouse device common for all mice
input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0
input: iMX6UL TouchScreen Controller as /devices/platform/soc/2000000.aips-bus/2040000.tsc/input/input1
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
pxp-v4l2 pxp_v4l2: initialized
imx2-wdt 20bc000.wdog: use WDOG_B to reboot.
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Key type dns_resolver registered
mmc1: MAN_BKOPS_EN bit is not set
Registering SWP/SWPB emulation handler
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
VSD_3V3: disabling
can-3v3: disabling
clk: Not disabling unused clocks
ALSA device list:
  No soundcards found.
Freeing unused kernel memory: 388K (80911000 - 80972000)
Starting UTP
uuc 0.5 [built Apr  1 2016 09:02:33]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh mksdcard.sh /dev/mmcblk1'
UTP: executing "sh mksdcard.sh /dev/mmcblk1"
“wait for /dev/mmcblk1 appear”
“wait for /dev/mmcblk1 appear”
“wait for /dev/mmcblk1 appear”
“wait for /dev/mmcblk1 appear”
“wait for /dev/mmcblk1 appear”
“wait for /dev/mmcblk1 appear”
“wait for /dev/mmcblk1 appear”
“wait for /dev/mmcblk1 appear”
“wait for /dev/mmcblk1 appear”
mmc1: Timeout waiting for hardware interrupt.
mmc1: switch to bus width 2 failed
mmc1: new DDR MMC card at address 0001
mmcblk1: mmc1:0001 P1XXXX 7.20 GiB
mmcblk1boot0: mmc1:0001 P1XXXX partition 1 2.00 MiB
mmcblk1boot1: mmc1:0001 P1XXXX partition 2 2.00 MiB
mmcblk1rpmb: mmc1:0001 P1XXXX partition 3 128 KiB
 mmcblk1: p1 p2
“wait for /dev/mmcblk1 appear”
1+0 records in
1+0 records out
1024 bytes (1.0 kB) copied, 0.280587 s, 3.6 kB/s
Checking that no-one is using thirandom: sfdisk urandom read with 20 bits of entropy available
s disk right now ... OK

Disk /dev/mmcblk1: 7.2 GiB, 773429 mmcblk1: p1 p2
6576 bytes, 15106048 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes

>>> Created a new DOS disklabel with disk identifier 0x8dd46570.
Created a new partition 1 of type 'W95 FAT32 (LBA)' and of size 500 MiB.
/dev/mmcblk1p2: Created a new partition 2 of type 'Linux' and of size 6.6 GiB.
/dev/mmcblk1p3:
New situation:

Device         Boot   Start      End  Sectors  Size Id Type
/dev/mmcblk1p1        20480  1044479  1024000  500M  c W95 FAT32 (LBA)
/dev/mmcblk1p2      1228800 15106047 13877248  6.6G 83 Linux

The partition table has been altered.
Calling ioctl() to re-read partition table.
Syncing disks.
UTP: sending Success to kernel for command $ sh mksdcard.sh /dev/mmcblk1.
utp_poll: pass returned.
UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=384 conv=fsync count=129'
UTP: executing "dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=384 conv=fsync count=129"
129+0 records in
129+0 records out
132096 bytes (132 kB) copied, 0.0373643 s, 3.5 MB/s
UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=384 conv=fsync count=129.
utp_poll: pass returned.
UTP: received command '$ echo 0 > /sys/block/mmcblk1boot0/force_ro'
UTP: executing "echo 0 > /sys/block/mmcblk1boot0/force_ro"
UTP: sending Success to kernel for command $ echo 0 > /sys/block/mmcblk1boot0/force_ro.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2'
UTP: executing "dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2"
718+0 records in
718+0 records out
367616 bytes (368 kB) copied, 0.161652 s, 2.3 MB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2.
utp_poll: pass returned.
UTP: received command '$ echo 1 > /sys/block/mmcblk1boot0/force_ro'
UTP: executing "echo 1 > /sys/block/mmcblk1boot0/force_ro"
UTP: sending Success to kernel for command $ echo 1 > /sys/block/mmcblk1boot0/force_ro.
utp_poll: pass returned.
UTP: received command '$ mmc bootpart enable 1 1 /dev/mmcblk1'
UTP: executing "mmc bootpart enable 1 1 /dev/mmcblk1"
UTP: sending Success to kernel for command $ mmc bootpart enable 1 1 /dev/mmcblk1.
utp_poll: pass returned.
UTP: received command '$ while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done '
UTP: executing "while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done "
UTP: sending Success to kernel for command $ while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done .
utp_poll: pass returned.
UTP: received command '$ mkfs.vfat /dev/mmcblk1p1'
UTP: executing "mkfs.vfat /dev/mmcblk1p1"
mkfs.fat 3.0.28 (2015-05-16)
UTP: sending Success to kernel for command $ mkfs.vfat /dev/mmcblk1p1.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk1p1'
UTP: executing "mkdir -p /mnt/mmcblk1p1"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p1.
utp_poll: pass returned.
UTP: received command '$ mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1'
UTP: executing "mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1"
UTP: sending Success to kernel for command $ mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/zImage'
UTP: executing "cp $FILE /mnt/mmcblk1p1/zImage"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/zImage.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/imx6ul-14x14-evk.dtb'
UTP: executing "cp $FILE /mnt/mmcblk1p1/imx6ul-14x14-evk.dtb"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/imx6ul-14x14-evk.dtb.
utp_poll: pass returned.
UTP: received command '$ umount /mnt/mmcblk1p1'
UTP: executing "umount /mnt/mmcblk1p1"
UTP: sending Success to kernel for command $ umount /mnt/mmcblk1p1.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext3 -E nodiscard /dev/mmcblk1p2'
UTP: executing "mkfs.ext3 -E nodiscard /dev/mmcblk1p2"
mke2fs 1.42.9 (28-Dec-2013)
Filesystem label=
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
434176 inodes, 1734656 blocks
86732 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=1778384896
53 block groups
32768 blocks per group, 32768 fragments per group
8192 inodes per group
Superblock backups stored on blocks:
        32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632

Allocating group tables: done                           
Writing inode tables: done                           
Creating journal (32768 blocks): done
Writing superblocks and filesystem accounting information: done

UTP: sending Success to kernel for command $ mkfs.ext3 -E nodiscard /dev/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk1p2'
UTP: executing "mkdir -p /mnt/mmcblk1p2"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2'
UTP: executing "mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2"
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk1p2): using internal journal
EXT3-fs (mmcblk1p2): mounted filesystem with ordered data mode
UTP: sending Success to kernel for command $ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2.
utp_poll: pass returned.
UTP: received command 'frf'
UTP: closing the file
UTP: sending Success to kernel for command frf.
utp_poll: pass returned.
UTP: received command '$ umount /mnt/mmcblk1p2'
UTP: executing "umount /mnt/mmcblk1p2"
UTP: sending Success to kernel for command $ umount /mnt/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ echo Update Complete!'
UTP: executing "echo Update Complete!"
Update Complete!
UTP: sending Success to kernel for command $ echo Update Complete!.
utp_poll: pass returned.

thanks for your support again ....

Best regards

Andy

0 Kudos

2,209 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

 

are you able to boot uboot ?

what bsp used in the case (please provide full name and link location),

please provide full log when linux fails to start

had you successfully programmed emmc with mfg tools ?

 

Best regards
igor

0 Kudos

2,209 Views
andyyang730
Contributor I

Hi igor

Sorry for reply you lately , but i still can not boot from EMMC now, i try to edit the uboot as the guide book get from NXP , but still can not work , there is nothing print out , but i can pass the ddr test....

here is new log catch when mfg burning the soft in to  emmc , hoping that can help you to analyze the issue

Stride=0 blocks, Stripe width=0 blocks
434176 inodes, 1734656 blocks
86732 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=1778384896
53 block groups
32768 blocks per group, 32768 fragments per group
8192 inodes per group
Superblock backups stored on blocks:  
        32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632
 
Allocating group tables: done                             
Writing inode tables: done                             
Creating journal (32768 blocks): done
Writing superblocks and filesystem accounting information: done  
 
UTP: sending Success to kernel for command $ mkfs.ext3 -E nodiscard /dev/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk1p2'
UTP: executing "mkdir -p /mnt/mmcblk1p2"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2'
UTP: executing "mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2"
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk1p2): using internal journal
EXT3-fs (mmcblk1p2): mounted filesystem with ordered data mode
UTP: sending Success to kernel for command $ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2.
utp_poll: pass returned.
random: nonblocking pool is initialized
^Ata block=0
Maximum filesystem blocks=1778384896
53 block groups
32768 blocks per group, 32768 fragments per group
8192 inodes per group
Superblock backups stored on blocks:  
        32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632
 
Allocating group tables: done                             
Writing inode tables: done                             
Creating journal (32768 blocks): done
Writing superblocks and filesystem accounting information: done  
 
UTP: sending Success to kernel for command $ mkfs.ext3 -E nodiscard /dev/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk1p2'
UTP: executing "mkdir -p /mnt/mmcblk1p2"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2'
UTP: executing "mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2"
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk1p2): using internal journal
EXT3-fs (mmcblk1p2): mounted filesystem with ordered data mode
UTP: sending Success to kernel for command $ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2.
utp_poll: pass returned.
random: nonblocking pool is initialized
32768 blocks per group, 32768 fragments per group
8192 inodes per group
Superblock backups stored on blocks:  
        32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632
 
Allocating group tables: done                             
Writing inode tables: done                             
Creating journal (32768 blocks): done
Writing superblocks and filesystem accounting information: done  
 
UTP: sending Success to kernel for command $ mkfs.ext3 -E nodiscard /dev/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk1p2'
UTP: executing "mkdir -p /mnt/mmcblk1p2"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2'
UTP: executing "mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2"
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk1p2): using internal journal
EXT3-fs (mmcblk1p2): mounted filesystem with ordered data mode
UTP: sending Success to kernel for command $ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2.
utp_poll: pass returned.
random: nonblocking pool is initializedrandom: nonblocking pool is initializedrandom: nonblocking pool is initialized
Error reading data on serial port:
  ŸÜŸø·ÃÎÊ¡£
 
 
 
 
 
U-Boot 2015.04-imx_v2015.04_4.1.15_1.0.0_ga+gd7d7c43 (Nov 15 2016 - 15:41:59)
 
CPU:   Freescale i.MX6UL rev1.1 at 396 MHz
CPU:   Temperature 56 C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C:   ready
DRAM:  512 MiB
MMC:   startingFSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment
 
Display: TFT43AB (480x272)
Video: 480x272x24
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc1(part 0) is current device
Net:   Phy 1 not found
PHY reset timed out
FEC1
Error: FEC1 address not set.
 
Boot from USB for mfgtools
Use default environment for                              mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot:  0  
Kernel image @ 0x80800000 [ 0x000000 - 0x552a38 ]
## Loading init Ramdisk from Legacy Image at 83800000 ...
   Image Name:   fsl-image-mfgtool-initramfs-imx6
   Image Type:   ARM Linux RAMDisk Image (gzip compressed)
   Data Size:    7565342 Bytes = 7.2 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 83000000
   Booting using the fdt blob at 0x83000000
   Using Device Tree in place at 83000000, end 8300b693
Modify /soc/aips-bus@02000000/bee@02044000:status disabled
ft_system_setup for mx6
 
Starting kernel ...
 
Booting Linux on physical CPU 0x0
Linux version 4.1.15-1.1.0-mfgtool+ga4d2a08 (bamboo@shlinux12) (gcc version 5.2.0 (GCC) ) #1 SMP PREEMPT Fri Apr 1 09:25:08 CST 2016
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board
cma: Reserved 320 MiB at 0x8c000000
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @8bb33000 s16768 r8192 d24192 u49152
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= clk_ignore_unused
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 173412K/524288K available (6895K kernel code, 319K rwdata, 2412K rodata, 388K init, 423K bss, 23196K reserved, 327680K cma-reserved, 0K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0xa0800000 - 0xff000000   (1512 MB)
    lowmem  : 0x80000000 - 0xa0000000   ( 512 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .text : 0x80008000 - 0x8091ef88   (9308 kB)
      .init : 0x8091f000 - 0x80980000   ( 388 kB)
      .data : 0x80980000 - 0x809cff00   ( 320 kB)
       .bss : 0x809d2000 - 0x80a3bf14   ( 424 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
        Additional per-CPU info printed with stalls.
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
------------[ cut here ]------------
WARNING: CPU: 0 PID: 0 at /home2/bamboo/build/4.1.X-1.0.0_ga/fsl-imx-x11/temp_build_dir/build_fsl-imx-x11/tmp/work-shared/imx6qdlsolo/kernel-mfgtool-source/arch/arm/mach-imx/gpc.c:581 imx_gpc_check_dt+0x4c/0x8c()
Modules linked in:
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.1.15-1.1.0-mfgtool+ga4d2a08 #1
Hardware name: Freescale i.MX6 Ultralite (Device Tree)
[<80015ee4>] (unwind_backtrace) from [<80012774>] (show_stack+0x10/0x14)
[<80012774>] (show_stack) from [<8068fc74>] (dump_stack+0x80/0xc8)
[<8068fc74>] (dump_stack) from [<80035f5c>] (warn_slowpath_common+0x74/0xb0)
[<80035f5c>] (warn_slowpath_common) from [<80036034>] (warn_slowpath_null+0x1c/0x24)
[<80036034>] (warn_slowpath_null) from [<8092c9fc>] (imx_gpc_check_dt+0x4c/0x8c)
[<8092c9fc>] (imx_gpc_check_dt) from [<8093c8e4>] (imx6ul_init_irq+0x8/0x18)
[<8093c8e4>] (imx6ul_init_irq) from [<80922328>] (init_IRQ+0x28/0x80)
[<80922328>] (init_IRQ) from [<8091fad8>] (start_kernel+0x210/0x3a0)
[<8091fad8>] (start_kernel) from [<8000807c>] (0x8000807c)
---[ end trace cb88537fdc8fa200 ]---
Outdated DT detected, suspend/resume will NOT work
mxc_clocksource_init 24000000
Switching to timer-based delay loop, resolution 41ns
sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80008280 - 0x800082f0
Brought up 1 CPUs
SMP: Total of 1 processors activated (48.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
device-tree: Duplicate name in lcdif@021c8000, renamed to "display#1"
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
mxs-dma 1804000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7392K (83800000 - 83f38000)
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) ?? 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
21c8000.lcdif supply lcd not found, using dummy regulator
mxsfb 21c8000.lcdif: failed to find mxc display driver  
Console: switching to colour frame buffer device 60x34
mxsfb 21c8000.lcdif: initialized
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 18, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 234, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
fsl-quadspi 21e0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff
fsl-quadspi 21e0000.qspi: Freescale QuadSPI probe failed
20b4000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 20b4000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 20b4000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 92:34:4a:77:13:9a
libphy: fec_enet_mii_bus: probed
fec 20b4000.ethernet eth0: registered PHC device 0
2188000.ethernet supply phy not found, using dummy regulator
pps pps1: new PPS source ptp1
fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: e6:1c:c3:1e:5c:d3
fec 2188000.ethernet eth1: registered PHC device 1
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
LUN: removable read only file: /fat
Number of LUNs=1
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
mousedev: PS/2 mouse device common for all mice
input: iMX6UL TouchScreen Controller as /devices/platform/soc/2100000.aips-bus/2040000.tsc/input/input0
snvs_rtc 20cc034.snvs-rtc-lp: snvs rtc: you use old dts file, please update it
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
pxp-v4l2 pxp_v4l2: initialized
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Key type dns_resolver registered
cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)
Registering SWP/SWPB emulation handler
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:08:17 UTC (497)
can-3v3: disabling
clk: Not disabling unused clocks
ALSA device list:
  No soundcards found.
Freeing unused kernel memory: 388K (8091f000 - 80980000)
Starting UTP
uuc 0.5 [built Apr  1 2016 09:02:33]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh mksdcard.sh /dev/mmcblk1'
UTP: executing "sh mksdcard.sh /dev/mmcblk1"
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
mmc1: MAN_BKOPS_EN bit is not set
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
a€?wait for /dev/mmcblk1 appeara€?
mmc1: Timeout waiting for hardware interrupt.
mmc1: switch to bus width 2 failed
mmc1: new DDR MMC card at address 0001
mmcblk1: mmc1:0001 P1XXXX 7.20 GiB  
mmcblk1boot0: mmc1:0001 P1XXXX partition 1 2.00 MiB
mmcblk1boot1: mmc1:0001 P1XXXX partition 2 2.00 MiB
mmcblk1rpmb: mmc1:0001 P1XXXX partition 3 128 KiB
 mmcblk1: p1 p2
a€?wait for /dev/mmcblk1 appeara€?
1+0 records in
1+0 records out
1024 bytes (1.0 kB) copied, 0.408099 s, 2.5 kB/s
Checking that no-one is using thirandom: sfdisk urandom read with 65 bits of entropy available
s disk right now ... OK
 
Disk /dev/mmcblk1: 7.2 GiB, 773429 mmcblk1: p1 p2
6576 bytes, 15106048 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
 
>>> Created a new DOS disklabel with disk identifier 0xaab3d726.
Created a new partition 1 of type 'W95 FAT32 (LBA)' and of size 500 MiB.
/dev/mmcblk1p2: Created a new partition 2 of type 'Linux' and of size 6.6 GiB.
/dev/mmcblk1p3:  
New situation:
 
Device         Boot   Start      End  Sectors  Size Id Type
/dev/mmcblk1p1        20480  1044479  1024000  500M  c W95 FAT32 (LBA)
/dev/mmcblk1p2      1228800 15106047 13877248  6.6G 83 Linux
 
The partition table has been altered.
Calling ioctl() to re-read partition table.
Syncing disks.
UTP: sending Success to kernel for command $ sh mksdcard.sh /dev/mmcblk1.
utp_poll: pass returned.
UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=384 conv=fsync count=129'
UTP: executing "dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=384 conv=fsync count=129"
129+0 records in
129+0 records out
132096 bytes (132 kB) copied, 0.0373955 s, 3.5 MB/s
UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=384 conv=fsync count=129.
utp_poll: pass returned.
UTP: received command '$ echo 0 > /sys/block/mmcblk1boot0/force_ro'
UTP: executing "echo 0 > /sys/block/mmcblk1boot0/force_ro"
UTP: sending Success to kernel for command $ echo 0 > /sys/block/mmcblk1boot0/force_ro.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2'
UTP: executing "dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2"
710+0 records in
710+0 records out
363520 bytes (364 kB) copied, 0.160146 s, 2.3 MB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2.
utp_poll: pass returned.
UTP: received command '$ echo 1 > /sys/block/mmcblk1boot0/force_ro'
UTP: executing "echo 1 > /sys/block/mmcblk1boot0/force_ro"
UTP: sending Success to kernel for command $ echo 1 > /sys/block/mmcblk1boot0/force_ro.
utp_poll: pass returned.
UTP: received command '$ mmc bootpart enable 1 1 /dev/mmcblk1'
UTP: executing "mmc bootpart enable 1 1 /dev/mmcblk1"
UTP: sending Success to kernel for command $ mmc bootpart enable 1 1 /dev/mmcblk1.
utp_poll: pass returned.
UTP: received command '$ while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done '
UTP: executing "while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done "
UTP: sending Success to kernel for command $ while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done .
utp_poll: pass returned.
UTP: received command '$ mkfs.vfat /dev/mmcblk1p1'
UTP: executing "mkfs.vfat /dev/mmcblk1p1"
mkfs.fat 3.0.28 (2015-05-16)
UTP: sending Success to kernel for command $ mkfs.vfat /dev/mmcblk1p1.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk1p1'
UTP: executing "mkdir -p /mnt/mmcblk1p1"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p1.
utp_poll: pass returned.
UTP: received command '$ mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1'
UTP: executing "mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1"
UTP: sending Success to kernel for command $ mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/zImage'
UTP: executing "cp $FILE /mnt/mmcblk1p1/zImage"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/zImage.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/imx6ul-14x14-evk.dtb'
UTP: executing "cp $FILE /mnt/mmcblk1p1/imx6ul-14x14-evk.dtb"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/imx6ul-14x14-evk.dtb.
utp_poll: pass returned.
UTP: received command '$ umount /mnt/mmcblk1p1'
UTP: executing "umount /mnt/mmcblk1p1"
UTP: sending Success to kernel for command $ umount /mnt/mmcblk1p1.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext3 -E nodiscard /dev/mmcblk1p2'
UTP: executing "mkfs.ext3 -E nodiscard /dev/mmcblk1p2"
mke2fs 1.42.9 (28-Dec-2013)
Filesystem label=
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
434176 inodes, 1734656 blocks
86732 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=1778384896
53 block groups
32768 blocks per group, 32768 fragments per group
8192 inodes per group
Superblock backups stored on blocks:  
        32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632
 
Allocating group tables: done                             
Writing inode tables: done                             
Creating journal (32768 blocks): done
Writing superblocks and filesystem accounting information: random: nonblocking pool is initialized
done
 
UTP: sending Success to kernel for command $ mkfs.ext3 -E nodiscard /dev/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk1p2'
UTP: executing "mkdir -p /mnt/mmcblk1p2"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2'
UTP: executing "mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2"
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk1p2): using internal journal
EXT3-fs (mmcblk1p2): mounted filesystem with ordered data mode
UTP: sending Success to kernel for command $ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2.
utp_poll: pass returned.

0 Kudos

2,209 Views
igorpadykov
NXP Employee
NXP Employee

are you able to boot this board from any other device

or for example run uboot with jtag ?

0 Kudos

2,209 Views
andyyang730
Contributor I

Dear Igor

due to we didn't set other device on our board, so can not try it .

could you share the mothond about how to run uboot with jtag?

thanks.

0 Kudos

2,209 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

uboot with jtag can be run in the same way as ddr tester on below link,
load uboot elf file to memory then start it
https://community.nxp.com/docs/DOC-105652

Best regards
igor

0 Kudos

2,208 Views
andyyang730
Contributor I

Hi igor

finally we startup the chip with changing BOOT_CFG2[7][6][5] to 000, but we are confused that why that need set to 1bit ,and not set to 8 bit?

thanks.

0 Kudos

2,208 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

are you able to boot uboot ?

what bsp used in the case (please provide full name and link location),

please provide full log when linux fails to start

had you successfully programmed emmc with mfg tools ?

Best regards
igor

0 Kudos

2,208 Views
andyyang730
Contributor I

Dear Igor

  • are you able to boot uboot ?

-->no , there is nothing print out ,when i power up the board

  • what bsp used in the case (please provide full name and link location),

-->i'm not make sure the version , and link now ...below is the folder info ,hoping that can help

    /home/baite/NXP/fsl-arm-yocto-bsp/build_gui/tmp/work/imx6ulevk-poky-linux-gnueabi/u-boot-imx/2015.04-r0/git

  • please provide full log when linux fails to start

-->there is nothing print out ...

  • had you successfully programmed emmc with mfg tools ?

-->yes , on last reply message i had provided log info ,and we can get 'DONE' when we use mfg tools , i think that is succeeded.

0 Kudos

2,209 Views
igorpadykov
NXP Employee
NXP Employee

could you try to extend POR (probably manually) up to 0.5-1 sec.

~igor

0 Kudos