Which i.MX6 audio module support audio right justified mode?
Case 1 : SSI (Synchronous Serial Interface) -> Audmux (Digital Audio MUX)
Case 2 : ESAI (Enhanced Serial Audio Interface)
None of these modules support the audio right justified mode. When SSI or ESAI operate in Master mode, the time slot length is always equal to the sample (word) lenght, configured in software. When SSI or ESAI operate in Slave mode, the settings should be made so as the sample (word) lenght, configured in software for these modules, would be equal to the length of the time slot, generated by an external Master.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------