QCVS PBL endianness output LS1012A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QCVS PBL endianness output LS1012A

Jump to solution
743 Views
nattapongsungch
Contributor III

Hello , I'm Nattapong. 

 

I'm working on LS1012ARDB and try to use GPIO1_xx and GPIO2_xx.

 

As i found on community, I have to change value at RCW.

 

I imported RCW file and adjust SDHC1_VSEL to GPIO1[23].

 

165781_165781.PNGqcvs.PNG

 

After generated PBL binary file looks like i got big endian if compare with original file.

 

165797_165797.pngpastedImage_2.png

[Left is original file, Right is change SDHC1_VSEL to GPIO1[23]]

 

 

 

 

Can I select endianness for output?.

 

 

Thank you

Nattapong 

Labels (1)
1 Solution
506 Views
addiyi
NXP Employee
NXP Employee

Use the drop down selection and select Quad SPI.

pastedImage_1.png

Adrian

View solution in original post

0 Kudos
3 Replies
506 Views
addiyi
NXP Employee
NXP Employee

Which version of QCVS you are using? If you use the latest available version, just select the RCW Sources as Quad SPI and PBL_swapped.bin will be generated.

Adrian

506 Views
nattapongsungch
Contributor III

Yes, I'm using latest  version (Version: 11.2.1 Build Id: 160913).  

How can i select RCW source ?.

Thank you.

Nattapong

0 Kudos
507 Views
addiyi
NXP Employee
NXP Employee

Use the drop down selection and select Quad SPI.

pastedImage_1.png

Adrian

0 Kudos