uboot 'bmp' command on iMX6Q SabreSD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot 'bmp' command on iMX6Q SabreSD

1,644 Views
andreacolomba
Contributor II

Hello, I would like to enable the 'bmp' and the 'hdmidet' commands on uboot on the iMX6Q SabreSD board.

At the moment I've been able to download and compile the uboot-imx sources from git following the tutorial: u-boot on the i.MX6 sabre sd platform in a few commands 

I read the uboot readme and I added the definitions of CONFIG_CMD_BMP and CONFIG_CMD_HDMIDETECT.

The definition I added are in /include/configs/mx6sabresd.h:

#define CONFIG_CMD_BMP

#define CONFIG_CMD_HDMIDETECT

I recompiled using 

  $ export CROSS_COMPILE=arm-linux-gnueabihf-

  $ make mx6qsabresd_config

  $ make

and then I put it on SD card to run. The board boots and displays a splashscreen on the connected HDMI.

But when I try to use 'hdmidet' command or 'bmp' command none of them works:

   Unknown command 'bmp' - try 'help'

   Unknown command 'bmp' - try 'help'

   

Using 'help' to display the commands doesn't show up 'bmp' nor 'hdmidet'.

Any suggestions?

Labels (1)
Tags (4)
0 Kudos
1 Reply

847 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andrea

seems CONFIG_SPLASH_SCREEN should be enabled in

include/configs/mx6sabresd.h:

#if defined(CONFIG_SPLASH_SCREEN) && defined(CONFIG_MXC_EPDC)
    /*
     * Framebuffer and LCD
     */
    #define CONFIG_CMD_BMP..

uboot-imx.git - Freescale i.MX u-boot Tree 

also one can post this to uboot mail list

U-Boot Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------