Question, USB Compliance Test of i.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, USB Compliance Test of i.MX6Q

890 Views
Aemj
Contributor IV

Dear team,

I would like to ask about the USB compliance test of i.MX6Q.

My customer is trying to measure eye-pattern of USB signals of i.MX6Q and they have a following question.

Referring to the following community thread, they are trying to measure eye-pattern of USB signal using with your i.MX6Q-SABRE board.

But after they executed the memtool command, Linux stopped and the signal did not flow out.

https://community.nxp.com/docs/DOC-105609

Their test environment is as below;

OS: LinuxBSP

Kernel: 3.14.28

Board: MCIMX6Q-SABRE

HW: Please see the attached file

 

After they executed following commands, Linux hung.

# memtool 0x2184184 1                           //read the register settings, address of the other USB port is 0x2184384

# memtool 0x2184184=0x18441205      // Force to output Test Packet for Eye Diagram Test   

# memtool 0x2184184=0x18411205      //Force to output J_STATE

# memtool 0x2184184=0x18421205      // Force to output K_STATE

# memtool 0x2184184=0x18431205      // Force to output SE0 (host) / NAK (device)

 

# memtool 0x2184384=0x18001305      // Force to output Reset

# memtool 0x2184384=0x18001285      //Ho Force to output Suspend

# memtool 0x2184384=0x18001245      // Force to output Resume

# memtool 0x2184184=0x18441205

 

Do you have any ideas on the cause of this phenomenon?

Thanks,

Miyamoto

Labels (1)
0 Kudos
1 Reply

497 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Miyamoto,

Please take a look at the following thread:

https://community.nxp.com/thread/383925

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos