mmdc command for Anroid M6.0 for MX6Q-SABRE-SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mmdc command for Anroid M6.0 for MX6Q-SABRE-SDB

596 Views
yuuki
Senior Contributor II

Dear all,


We run Android M6.0 on SABRE-SDB.

   BSP: IMX6_M6.0.1_2.1.0_ANDROID_SOURCE_BSP (REV M6.0.1_2.1.0)

We want to use mmdc command.
However, we cannot use mmdc command.

The following error occurs.
===========================
root@sabresd_6dq:/ # mmdc
Could not open /dev/mem
===========================


Would you tell me the method using mmdc command on Android M6.0?

May I have advice?

Best Regards,
Yuuki

Labels (2)
Tags (2)
0 Kudos
3 Replies

409 Views
art
NXP Employee
NXP Employee

So, does it work finally?

Best Regards,

Artur

0 Kudos

409 Views
yuuki
Senior Contributor II

Dear Artur-san,

Yes, it worked without a problem.

Best Regards,

Yuuki

0 Kudos

409 Views
yuuki
Senior Contributor II

I'm sorry.


We noticed that we did not make config of kernel Enable.

A problem was settled by making config of kernel Enable.

Best Regards,
Yuuki

0 Kudos