codeworriror 5.1版本在win10 升级后无法识别BDM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codeworriror 5.1版本在win10 升级后无法识别BDM

2,301 Views
wuyurong
Contributor I

系统情况:codeworriror 5.1版本,Win10 系统(已完成最近一次升级)。问题描述:设备管理器无法识别 DBM,只能通过添加过期硬件添加为:OPEN SOURCE BDM-JM60,且更新驱动程序时无法安装USBDM_BDM_Interface.inf,硬件管理器提示不能安装32位驱动。在CodeWorrior中下载时显示“Device not responding”。在此之前,我已成功安装并能顺利下载单片机程序。

163888_163888.pngcant find DBM1.png164633_164633.pngcant find DBM2.png

Labels (1)
0 Kudos
2 Replies

1,481 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi ,

1. The CW v5.1 not support Win10 .

pastedImage_1.png

While the CWv5.2 support Win10 .

pastedImage_2.png

Which chip do you use ?  CW5.2 can support:

 

    - MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96

    - MC9S12G128, MC9S12G96

    - MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64

    - MC9S12GN16, MC9S12GN32

    - MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128

    - MC9S12XEP100, MC9S12XEP768

    - MC9S12XEQ384, MC9S12XEQ512

    - MC9S12XET256

    - MC9S12XS128, MC9S12XS256, MC9S12XS64

    - MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64

2.  Please download the latst USBDM driver : USBDM - Browse Files at SourceForge.net 

  There is a thread about USBDM for CW v5.2 ,you can refer to : https://community.nxp.com/message/607593 

Hope it helps

Alice

0 Kudos

1,481 Views
wuyurong
Contributor I

Your suggest helps nothing, I solved it by another way cause it was caused by another system updating issue. Any way, thank you all the same.

0 Kudos