About Imx6qSabresd board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Imx6qSabresd board

1,162 Views
vvjay
Contributor I

I once successfully built ZImage、Rootfs、.imx .dtb file and flash them into emmc, and everything was ok(one month ago). But this time, i change the kernel and recompile it , build is ok, no error. But this  time after i flash them into emmc, i can't find unit test package in the root direction, and ssh also disappear(i use putty to ssh the board) , and i tftp mxc_vpu_test.out file to the board and execute it, it say no libvpu.so.4 , i think it not vpu lib.    But  i follow the steps what i did one month age, and didn't change anything.   i use mfgtool to flash it ,   even i use the old files(what i built one month ago),   it is still same.  

i delete the charge-led driver in the new one , so i can confirm i flash the old one cause charge-led driver still in the /sys/class/leds/ dir. Can anyone tell me,   what may happened and how to solve it.

I use Imx6QSABRESD BOARD.    kernel version:  core-image-base     linux: YOCTO

THANK YOU!

Jay

Labels (1)
Tags (1)
0 Kudos
1 Reply

848 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jay

please check yocto faq:

https://community.nxp.com/docs/DOC-94023
https://community.nxp.com/thread/376369

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------