Hello,Community:
I am now working on Freescale imx6q connected a 7" 800 x 480 LCD display and touch with tsc2007, i change the file .dtis .
if i use a mouse the display is ok ,the touch can work but not the correct position. but if i run the ts_calibrate int /usr/bin first i can calibrate the touch panel,but after ts_calibrate quit the lcd has a wrong display, the command cat .bmp bf0 also display wrong ,but if i run ts_calibrate or ts_test,the lcd is ok.
Are you using LCD in "rotated" mode?
Please try to play with xrandr prior to ts_calibrate.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thankyou for your answer, my lcd was not in "rotated" mode.you can see my pictures of the screen. when i run ts_calibrate the screen will be ok again