questiong about AIPS(chapter 13) and AHB-to-APBH Bridge(chapter 14)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

questiong about AIPS(chapter 13) and AHB-to-APBH Bridge(chapter 14)

2,432 Views
yangweihuadiand
Contributor I

I  am reading IMX6DQRM, have a questiong about AIPS(chapter 13)  and AHB-to-APBH Bridge(chapter 14), is APB difference for IP BUS? and APB is only used in GPMI?

thanks!

Labels (1)
0 Kudos
2 Replies

1,581 Views
igorpadykov
NXP Employee
NXP Employee

Hi

you are right APB is only used for GPMI, actually

it came from i.MX23/28 processors.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,581 Views
yangweihuadiand
Contributor I

thanks a lot.

many ARM SOC manufacturers use APB to connect peripheral(APB is a ARM standard),

NXP(fsl) use his private IP bus to do this?

0 Kudos