microSD write operation hangs on P4080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

microSD write operation hangs on P4080

2,768 Views
yogesh_ahiray
Contributor I

Hi All,

We are using Kernel 3.0.34 ( from SDK 1.2) on our  P4080 board. We are using microSD card and have our filesystem on it.

The Write operation on SD card randomly hangs and eventually Kernel causes following exception, The same can be reproduce if we write continuously on uSD card with dd command.

INFO: task dd:2184 blocked for more than 120 seconds.

"echo 0 > /proc/sys/kernel/hung_task_timeout_secs" disables this message.

dd              D 0ff1d604     0  2184   2163 0x00000000

Call Trace:

[c7401940] [00000003] 0x3 (unreliable)

[c7401a00] [c0007654] __switch_to+0x94/0xc0

[c7401a20] [c0607068] __schedule+0x268/0x610

[c7401b50] [c0607860] schedule+0x30/0xd0

[c7401b60] [c01ac8d4] do_get_write_access+0x2c4/0x470

[c7401bd0] [c01acc00] jbd2_journal_get_write_access+0x30/0x60

[c7401be0] [c0191658] __ext4_journal_get_write_access+0x38/0xa0

[c7401c00] [c0174010] ext4_reserve_inode_write+0x90/0xc0

[c7401c20] [c0174068] ext4_mark_inode_dirty+0x28/0x1b0

[c7401c50] [c0179718] ext4_dirty_inode+0x38/0x70

[c7401c60] [c010ca3c] __mark_inode_dirty+0x3c/0x220

[c7401c80] [c0117294] generic_write_end+0xe4/0x110

[c7401ca0] [c0177ad4] ext4_da_write_end+0x1a4/0x370

[c7401ce0] [c00a637c] generic_file_buffered_write+0xdc/0x230

[c7401d50] [c00a6ef8] __generic_file_aio_write+0x238/0x4d0

[c7401dc0] [c00a7218] generic_file_aio_write+0x88/0x150

[c7401e10] [c016cff4] ext4_file_write+0x134/0x330

[c7401e60] [c00e2c68] do_sync_write+0xa8/0x130

[c7401ef0] [c00e35a8] vfs_write+0xa8/0x1a0

[c7401f10] [c00e391c] sys_write+0x4c/0x90

[c7401f40] [c000f340] ret_from_syscall+0x0/0x3c

--- Exception: c01 at 0xff1d604

    LR = 0x100044c8

Kernel panic - not syncing: hung_task: blocked tasks

Call Trace:

[e6743ea0] [c0007d64] show_stack+0x44/0x160 (unreliable)

[e6743ee0] [c060a4d0] panic+0xac/0x1ec

[e6743f40] [c008f254] watchdog+0x254/0x270

[e6743fa0] [c0065fdc] kthread+0x7c/0x80

[e6743ff0] [c000e208] kernel_thread+0x4c/0x68

More Information::::

After looking into uSD card messages ( enabled SD/MMC debug logs) the SD card continuously responds with following messages and never completes its write operation,

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001

mmc0: req done (CMD13): 0: 00000c00 00000000 00000000 00000000

mmc0: starting CMD13 arg aaaa0000 flags 00000195

I am using Kingston 8GB and tried other cards like Toshiba, Lexar etc they all fails at some point of time.

Any help will be highly appreciated, this is causing us major block now.

Thanks

Yogesh 

Tags (4)
0 Kudos
4 Replies

652 Views
diegowarszawski
Contributor I

This is the link to the question 

https://community.nxp.com/thread/315660 

0 Kudos

652 Views
ToniZollikofer
NXP TechSupport
NXP TechSupport

This is a duplicate. The question was re-submitted in the correct community and already answered. Sorry, don´t know how to remove duplicates.

0 Kudos

652 Views
aananthcn
Contributor II

Can you please let us know the link for the original question?

0 Kudos

652 Views
aananthcn
Contributor II

Can you please let us know the link for the duplicate question?

0 Kudos