I have a question about Out of Reset Condition of ENET1_RX_DATA0(F16)pin of i.MX6UL.
I seem that the description of Datasheet is different from register explanation of Reference Manual.
In Datasheet,
The Out of Reset Condition of ENET1_RX_DATA0(F16)pin is ALT5/ENET1_RX_DATA0.
In Reference Manual,
The Reset value of MUX_MODE field in IOMUXC_SW_MUX_CTL_PAD_ENET1_RX_DATA0 register is "ALT5 mux port: GPIO2_IO00".
Which description is correct?
Best Regards,
Yuuki
Solved! Go to Solution.
The datasheet is not correct, that pin's default function is ALT5, GPIO2_IO00, not ENET1_RX_DATA0.
The correct value is the ALT5 GPIO2_IO00 value, as described in the Reference Manual document. The ALT0 value, given in the Data Sheet document, is just a typo.
Have a great day,
Artur
The datasheet is not correct, that pin's default function is ALT5, GPIO2_IO00, not ENET1_RX_DATA0.