How to update DDR3 calibration Result in U-boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to update DDR3 calibration Result in U-boot?

538 Views
hrushinale
Contributor III

For our customized board running on i.MX6 dualite  ,we have 2GB RAM.The RAM part number is MT41K256M16TW-107 which is from Micron.We are using U-boot 2014.04.We run the DDR stress test and its successful.But I dont know where to update these values in U-boot so that I can run the U-boot on Dualite Board?

Thanks & Regards,

Hrushi

Tags (2)
0 Kudos
1 Reply

367 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following

How to use DDR3 Calibration Values

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos