BSP cloning wizard MQX 4.2 problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP cloning wizard MQX 4.2 problem

Jump to solution
859 Views
arnogir
Senior Contributor II

Hello,

I want use BSP cloning wizard to create my own Specific target OS.

I followed instruction given in this post:

bsp cloning wizard MQX 4.2

But on step 3, on the field "Board base" I have not choice, the list is empty. Then I can't continue...

Is anybody has an idea?

0 Kudos
1 Solution
583 Views
arnogir
Senior Contributor II

Hello,

I'm using Windows 10.

MQX 4.2 is installed in the default folder (c:\Freescale\Freescale_MQX_4_2)

I have just found how resolve this problem.

In Settings/Preferences, I clicked on "Restore defaults" button.

This make no change in the windows because my folders was already the default folder.

But after do "Apply" then "Ok", the list in "Board base" filed appears filled now!

...

View solution in original post

0 Kudos
3 Replies
583 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Arnaud:

What host operating system you are using? Windows 7, 8 or 10?

In addition, I suggest install MQX in the default folder.

Regards

Daniel

0 Kudos
584 Views
arnogir
Senior Contributor II

Hello,

I'm using Windows 10.

MQX 4.2 is installed in the default folder (c:\Freescale\Freescale_MQX_4_2)

I have just found how resolve this problem.

In Settings/Preferences, I clicked on "Restore defaults" button.

This make no change in the windows because my folders was already the default folder.

But after do "Apply" then "Ok", the list in "Board base" filed appears filled now!

...

0 Kudos
583 Views
csmgsarma
Contributor IV

Hi danielchen

I have am using windows 10, KDSV3 and MQX4.2 for TWR64 board. I am not able to run BSP Cloning Whizard. I see this error:
pastedImage_1.png

Based on the readme file(location: C:\Freescale\Freescale_MQX_4_2\tools\BSPCloningWizard\readme), I have installed latest JRE(jre-8u144-windows-x64.exe) and updated it. Am I missing something? 

I had tried to run the BSP cloning  wizard patch(FSLMQXOS_4_1_1_GA_UPDATE_BSPCW_1_5_GA.exe) but it seems to be looking for MQX V4.1 and as i am on MQX4.2, it didnt execute. Here's a  screenshot:

pastedImage_2.png

Am I missing something? 

Thanks in anticipation.

Best regards
Sarma

0 Kudos