I have recently upgraded from 4.1 to MQX 4.2 and I am still using CodeWarrior for MCU
Version: 10.6
When I try to create a project the option from the drop down shows MQX 4.1 and the Select Board
Dialog box is empty. It would appear that CodeWarrior is still pointing to the old 4.1 folder. Where
is this option located and how do I setup CodeWarrior to use MQX 4.2 folder and options?
David
Hello David
Please follow the below steps:
1. Go to Help->Install New Software
2. In the work with space select FSL MCU Eclipse Update Site - http://freescale.com/lgfiles/updates/Eclipse/MCU10_6/com.freescale.mcu.updatesite
3. Select MCU v10.6 Updates for MQX and click next (follow the steps to complete the operation)
4. After install the plug-ins, restart CodeWarrior. At this point you should be able to create a new MQX project.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Sol,
I have got same problem like David, but your suggestions are not helping me. Maybe it is because i am using Windows 10, 64 bits machine and 10.6.4 IDE, Professional licence. What you could advice me to do?
Bosko