IMX6DQ firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DQ firmware

566 Views
khaledali
Contributor III

I want to know if IMX6DQ series have the same firmware code which is  on the ROM chip ?
and
Is it an open source firmware that i can read and modify ?
and
If yes can anyone give me a link to read from ? !

Labels (1)
0 Kudos
3 Replies

418 Views
igorpadykov
NXP Employee
NXP Employee

Hi Khaled

ROM sources are not open source and can not be changed,

also sources are not available for customers, sorry.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

418 Views
khaledali
Contributor III

Ok is there any way to put any other firmware on the ROM chip ?

0 Kudos

418 Views
igorpadykov
NXP Employee
NXP Employee

no, as ROM is one time programmable memory.

~igor