vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
[Playing ][Vol=01][01:07:27/01:31:03][fps:0]vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
Aborted by signal Interrupt...
VS0 destroyed, force=0!
[--->FINALIZE isink
hwbuf allocator zone(356352) destroied.
[--->FINALIZE aiurdemux
fsl_player_stop()
player_exit(): No more multimedia files, exit.
root@phyBOARD-SUBRA-iMX6:/mnt
Hi Nagamahesh
please look at suggestions provided on
Getting vss/mfw_gst_vss_common.c:1003 ioctl error, return -1
https://bugzilla.yoctoproject.org/show_bug.cgi?id=5331
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Our main requirement was to playback any mp4 video with resolution of 1024x768 @50 Hz on i.MX6-SOLO .
$gplay Demo.MP4
is the command which we are giving to play the video.
The Video type is MPEG-4 video (video/mp4) and Video Codec is H.264 and Audio Codec is MPEG-4 AAC.
The Images are built with PTXdist buildsystem, We are assuming memory leak with these Images.
We tried to play the MP4 video with different resolutions.
When we played MP4 video with 720 x 480 resolution of 2 minute length, the occupied memory is getting free from RAM.
So, we thought playing high resolution video is the issue, as we earlier played 1280*720 resolution of 1.01 hour length video .
But when we played MP4 videos with different resolution of 1 hour length, we faced the same issue, but now the memory
consumption by RAM is slow for less resolution videos.
We checked the memory consumption with free command.
old BSPs have problems with memory leak, please try with latest nxp BSPs on:
i.MX 6 Series Software and Development Tool|NXP
~igor
Hi Igor,
I have tested on the latest Ycoto BSP with the below command, but the HD video is playing very slow and got below error:
$gst-launch-1.0 filesrc location=Demo.mp4 ! qtdemu ! h264parse ! v4l2video1dec ! videoconvert ! videoscale ! fbdevsink sync=trueux
*****************************************************************************************************************
WARNING: from element
/GstPipeline:pipeline0/GstFBDEVSink:fbdevsink0: A lot of buffers are
being dropped.
Additional debug info:
PD15.3.0/build/tmp-glibc/work/cortexa9hf-vfp-neon-phytec-linux-gnueabi/gstreamer1.0/1.4.5-r0/gstreamer:
There may be a timestamping problem, or this computer is too slow.
********************************************************************************************************************