How to use the EPDC on the iMX6SLEVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the EPDC on the iMX6SLEVK

Jump to solution
1,957 Views
miaobai
Contributor I

     I need to drive a EPD with the iMX6SLEVK.  I connect the pins to EPDC expansion port on iMX6SLEVK as follow .

      EPD  pins                                                        ------  iMX6SLEVK expansion port

      VCOM                                                              ------  EPDC_VCOM0

      BORDER                                                        ------  EPDC_BDR0

      D0~D15                                                           ------  EPDC_D0~EPDC_D15

      CKH(clock source driver)                                ------ EPDC_SDCLK_P

      LEH(latch enable source driver)                      ------ EPDC_SDLE

      OEH(output enable source driver)                  ------ EPDC_SDOE

      STH(start pulse source driver)                        ------ ?

     MODE1(output mode selection gate driver)     ------ ?

     STV(start pulse gate driver)                              ------ EPDC_GDSP

     CKV(clock gate driver)                                      ------ EPDC_GDCLK

    

Now,my questions :

1     There are two pins I don't know how to connect.

2     Is right the other pins out?

3    How to use the last some pins on EPDC expansion port on iMX6SLEVK like EPDC_PWRCTRL  EPDC_SDCE etc?

4   Where can I find the reference design of the IMXEBOOKDC3-E?

Thank you!

Labels (1)
Tags (2)
0 Kudos
1 Solution
1,291 Views
art
NXP Employee
NXP Employee

1. STH(start pulse source driver)    --------    EPDC_SDCE0

MODE1(output mode selection gate driver)  --------    EPDC_GDRL

2. Yes, this is right.

3. Just leave them floating.

4. This documentation is not publicly available due to NDA with E-Ink.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
1,292 Views
art
NXP Employee
NXP Employee

1. STH(start pulse source driver)    --------    EPDC_SDCE0

MODE1(output mode selection gate driver)  --------    EPDC_GDRL

2. Yes, this is right.

3. Just leave them floating.

4. This documentation is not publicly available due to NDA with E-Ink.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,055 Views
Ryder
Contributor I

Hi

Thanks for your great topic and support

According to this topic, I have successfully connected my EPD to the IMX6SLEVK, except for 1 pin

It's called CPV(Shift clock input), pls check the attached image for a more detailed description

EPD connection.png

 

Could you please check and tell me how to do it right?

 

Thanks

Ryder

 

0 Kudos