Host PC: windows 10 OS Build 10586.420
IAR Ver: IAR Embedded Workbench for ARM 7.70.1.1
Board: FRDM-KW24D
CMSIS-DAP Drivers instaled: Windows serial configuration - Handbook | mbed
so i got this
Lounch IAR
open workspace:
C:\Freescale\Kinetis_BeeStack_5.0.0\examples\zigbee_HaDimmableLight_OtaClient\kw2x\frdmkw24\freertos\iar
zigbee_HaDimmableLight_OtaClient_frdmkw24_freertos_Zed_Rs.eww
Note: here there is one that by default come wiht J-Link in the debug configuration i use that come with CMSIS-DAP by default it compile without error or warnings.
Then Click on: Donwload and debug
D1 on board (FRDM-KW24D green led) start flash fast and took around 5 minuts to have thist result:
Fri Jun 24, 2016 13:14:35: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.5\arm\config\debugger\NXP\KW2xD.dmac(103,17): Error: Operation error.
Fri Jun 24, 2016 13:14:35: Error while calling macro execUserCoreConnect
Fri Jun 24, 2016 13:15:31: Fatal error: Failed to connect to CPU Session aborted!
Fri Jun 24, 2016 13:15:31: IAR Embedded Workbench 7.70.1 (armproc.dll)
Fri Jun 24, 2016 13:15:31: Loading the CMSIS-DAP driver
I try this with 4 diferent board FRDM-KW24D with the same results.
then i try change systematic all params check box on
-project
- options
- Debugger
and CMSIS DAP
always with the same results
Hi,
Please make reference from this post:FRDM-KW24D512 non-responsive after bootload .
Hi Fang LI
It didnt bootload. i test it in:
Updating. I download from OpenSDA Serial and Debug Adapter|NXP
So looking https://mcuoneclipse.com/ how to recovery find and do like i say in this post FRDM-KW24D512 OpenSDA not responding
Note: all previous in Windows 7.
Trying again and trying ................ 1) Default firmware application 2) Latest firmware application 3)P&E Any OpenSDA for KW
Brick and unbrick process
*
*
Eureca from Sagger TWR-KW24D512 It Work. remeber this process most be done from Windos 7 or XP