No rule to make target `mx28evk_nand_defconfig'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No rule to make target `mx28evk_nand_defconfig'

Jump to solution
1,477 Views
ethanjunechu
Contributor I

system: ubuntu10.04

lib: L2.6.35_1.1.0_130130_source

ERR:No rule to make target `mx28evk_nand_defconfig'

ethan@ubuntu:~/Desktop/ltib$ ./ltib

Processing platform: Freescale iMX28 Based Boards

===================================================

using config/platform/imx/.config

Processing: fake-provides

===========================

Processing: u-boot

====================

Build path taken because: directory build, no prebuilt rpm,

scbuild/scdeploy already unpacked package

Processing: u-boot

====================

Build path taken because: directory build, build key set, no prebuilt rpm,

rpmbuild --dbpath /home/ethan/Desktop/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/ethan/Desktop/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/ethan/Desktop/ltib/tmp' --define '_rpmdir /home/ethan/Desktop/ltib/rpm/RPMS'  --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit  /home/ethan/Desktop/ltib/tmp/u-boot.spec

Building target platforms: arm

Building for target arm

Executing(%build): /bin/sh -e /home/ethan/Desktop/ltib/tmp/rpm-tmp.36157

+ umask 022

+ cd /home/ethan/Desktop/ltib/rpm/BUILD

+ cd u-boot-2009.08

+ : mx28_evk_config

+ eval echo

+ echo

+ PKG_U_BOOT_PATH_PRECONFIG=

+ SRC_DIR=/home/ethan/Desktop/ltib/rpm/BUILD/u-boot-2009.08

+ BUILD_DIR=/home/ethan/Desktop/ltib/rpm/BUILD/u-boot-2009.08

+ [ /home/ethan/Desktop/ltib/rpm/BUILD/u-boot-2009.08 != /home/ethan/Desktop/ltib/rpm/BUILD/u-boot-2009.08 ]

+ cd /home/ethan/Desktop/ltib/rpm/BUILD/u-boot-2009.08

+ [ -n  ]

+ make HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ CROSS_COMPILE=arm-none-linux-gnueabi- O=/home/ethan/Desktop/ltib/rpm/BUILD/u-boot-2009.08 mx28_evk_config

make: *** No rule to make target `mx28_evk_config'.  Stop.

error: Bad exit status from /home/ethan/Desktop/ltib/tmp/rpm-tmp.36157 (%build)

RPM build errors:

    Bad exit status from /home/ethan/Desktop/ltib/tmp/rpm-tmp.36157 (%build)

Build time for u-boot: 0 seconds

Failed building u-boot

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Sun Jul  3 18:28:37 2016

Ended:   Sun Jul  3 18:28:37 2016

Elapsed: 0 seconds

These packages failed to build:

u-boot

Build Failed

Exiting on error or interrupt

Labels (1)
0 Kudos
1 Solution
1,200 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ethan

please look at solution for this error

LTIB build errors i.MX6Q

Also if there are several builds for other processors, recommended

to try fresh VM for building with i.MX28 processor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
1,201 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ethan

please look at solution for this error

LTIB build errors i.MX6Q

Also if there are several builds for other processors, recommended

to try fresh VM for building with i.MX28 processor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,200 Views
ethanjunechu
Contributor I

Thanks for the answer, it maybe useful.But, I try on the ubuntu 12.04,it`s ok now.:smileyhappy:

0 Kudos