The STANDBY mode of MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The STANDBY mode of MPC5748G

1,487 Views
binbinwu
Contributor II

Hi,

I want to know whether MPC5748G can run in a loop that changeing from DRUN mode to STANDBY mode.

Just like the following code, from RUN3 mode to STOP mode.

155092_155092.pngpastedImage_1.png

Thank you very much for your help.

 

Wu Binbin

Labels (1)
5 Replies

917 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, it is possible to enter STANDBY mode from DRUN.

I have shared simple example using STM_0 for wake up here:

Example MPC5748G Standby mode GHS614

Regards,

Lukas

917 Views
Besir
Contributor I

Hi Lukas,

Could you share the attachment Example MPC5748G Standby mode GHS614 

Thanks

0 Kudos

917 Views
binbinwu
Contributor II

Hi,

Lukas, thank you for your help. And I want to konw whether MPC5748G can change from DRUN to STANDBY, then to DRUN , then to STANDBY and so on.

Is it necessary before enter STANDBY mode?

pastedImage_0.png

After configure STANDBY, if I just use the following codes, can I enter STANDBY mode?

pastedImage_1.png

Regards,

Binbin

917 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

It's example only. Of course, it is not necessary to use push button to enter STANDBY mode, so it is not necessary to configure the PA1 pad. Just modify it as you need.

Yes, that sequence is use to enter STANDBY.

Regards,

Lukas

917 Views
binbinwu
Contributor II

Hi,

Lukas, thank you for your help.

In the Application Note: AN2865, there are something about Low Power(MPC56××B/S).
pastedImage_1.png

It says that after the first wakeup timeout, mode changes from STANDBY to DRUN. But we can't go back to STANDBY because of the reasons in the red circle. It uses the STOP mode to repalce STANDBY mode. I want to konw whether MPC5748G is the same with MPC56××B/S. Can MPC5748G go back to STANDBY after changing from STANDBY to DRUN?

Regards,

Binbin

0 Kudos