On IPU Base address in imx6qdl.dtsi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

On IPU Base address in imx6qdl.dtsi

Jump to solution
778 Views
gaun
Contributor II

Hi,

Is there a typo in the in the base address of the IPU in imx6qdl.dtsi? The base address should have been 0x02600000 and not 0x02400000, right?

For reference:

linux-fslc/imx6qdl.dtsi at patches-4.1 · Freescale/linux-fslc · GitHub

I verified in the reference manuals and I don't find the IPU memory map at 0x02400000. Please verify.

Thanks.

Labels (4)
0 Kudos
1 Solution
634 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following

About imx6d ipu base address different in RM. and device tree.

Have a great day,
Yuri
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
635 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following

About imx6d ipu base address different in RM. and device tree.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos