Hello,
I want to debug on board K22 microcontroller on my FRDM-K22F board using CodeWarrior, however I am having this error:
My debug configuration for CodeWarrior is as follows. I cannot change "Erase Options". No matter what I select, the next time I open the dialog, it resets back to "Block erase entire device".
I have a new FRDM-K22F board and I have programmed it with USBDM using "OpenSDAv2_1_Unique_ID.bin" file under the folder "../pgo/USBDM 4.12.1.100/FlashImages/MKxx".
The board is listed fine in the Device Manager, as it can be seen in below screenshot:
Codewarrior also shows that the USBDM plugins are installed:
I can also, with no errors, detect, program and verify the chip using "ARM Programmer" tool of USBDM:
What could possible be my problem? Why I cannot debug it using CodeWarrior?
Solved! Go to Solution.
Hello ,
As i know , the chip of FRDM-F22 board is MK22FN512VLH12 MCU,
while the CWv10.6 doesn't support this chip .
You can use the KDS v3.2 to develop this chip .
Please refer to this thread to download and install :
New Kinetis Design Studio v3.2.0 available
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello ,
As i know , the chip of FRDM-F22 board is MK22FN512VLH12 MCU,
while the CWv10.6 doesn't support this chip .
You can use the KDS v3.2 to develop this chip .
Please refer to this thread to download and install :
New Kinetis Design Studio v3.2.0 available
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Oh, silly me. You are right.
Thank you very much for this help.. :smileyhappy:
Hi Abdullah,
Welcome !
BR
Alice