I can't read the session register in NT3H1101 from RF side with a PN532.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can't read the session register in NT3H1101 from RF side with a PN532.

1,285 Views
lakeliu
Contributor I

I want to read data from NT3H1101 with a PN532(WORK IN PASS-THROUGH MODE).  The READ and WRITE instructions execute successfully,  but the instructions GET_VERSIONFAST_READ and SECTOR SELECT don't execute successfully

for example:

//WRITEsuccessfully:

PC->PN53200 00 FF 09 F7 D4 40 01 A2 0c aa aa aa aa 95 0

PN532->PC00 00 FF 00 FF 00 00 00 FF 03 FD D5 41 00 EA 00

//READsuccessfully:

PC->PN53200 00 FF 05 FB D4 40 01 30 0c af 00

PN532->PC00 00 FF 00 FF 00 00 00 FF 13 ED D5 41 00 AA AA AA AA 00 00 00 00 00 00 00 00 00 00 00 00 42 00

//GET_VERSIONnot successfully:

PC->PN53200 00 FF 04 Fc D4 40 01 60 8b 00

PN532->PC00 00 FF 00 FF 00 00 00 FF 01 FF 7F 81 00

//FAST_READnot successfully:

PC->PN53200 00 FF 00 00 FF 06 Fa D4 40 01 3a 0c 0f d0 00

PN532->PC:no answer

// SECTOR SELECTnot successfully:

PC->PN53200 00 FF 07 F9 D4 40 01 c2 ff 16 fb 19 00

PN532->PC00 00 FF 00 FF 00 00 00 FF 03 FD D5 41 13 D7 00

PC->PN53200 00 FF 09 F7 D4 40 01 03 00 00 00 36 cd e5 00

PN532->PC 00 00 FF 00 FF 00 00 00 FF 01 FF 7F 81 00

READ ADDRESS 0XF8

PC->PN53200 00 FF 07 F9 D4 40 01 30 f8 2d fc 9a 00

PN532->PC00 00 FF 00 FF 00 00 00 FF 03 FD D5 41 01 E9 00

0 Kudos
1 Reply

747 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello lake liu:

The GET_VERSION and FAST_READ are not NFC Forum standard commands, so these are not recognized by the InDataExchange command you are using (0x40). But the tag can work anyway by using the InCommunicateThru command instead (0x42). See below for an example:

// GET_VERSION

00 00 FF 04 FC D4 40 01 60 8B 00 :smileyx:

00 00 FF 03 FD D4 42 60 8A 00 :smileycheck:

To use the InCommunicateThru command the card has to be activated first with the InListPassiveTarget command, which will configure as well the required RF protocol settings.

Also consider that the PN532 will not receive a CRC after sending SECTOR_SELECT command. See the next discussion:

NTAG I²C Sector Select on PN532

I hope this helps.


Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos