Can I  get  the UART using example on MPC5607B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I  get  the UART using example on MPC5607B

652 Views
spring236869
Contributor I

Can I  get  the example of UART  using  on MPC5607B ? 

When  I use UART mode  on MPC5607B,  the stop bit is low ,why? 

 

154155_154155.pngpastedImage_0.png

Labels (1)
0 Kudos
1 Reply

460 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

this example uses UART:

Example MPC5604B PinToggleStationery CW210

And attached you will find next two sample codes.

All of them are written for MPC5604B but there are no differences in case of UART.

Regards,

Lukas

0 Kudos