Want to serial download from UART of MCIMX6UL-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Want to serial download from UART of MCIMX6UL-EVK

2,129 Views
ko-hey
Senior Contributor II

Hi all

My customer use MCIMX6UL-EVK and want to download a image to eMMC over UART.

We found a following thread and tried it but can not succeed.

i.MX USB Loader

Can the "imx_usb_loader(imx_uart)" use with MCIMX6UL-EVK ?

If yes, please tell me how to modify the configuration file.

Ko-hey

Labels (1)
0 Kudos
4 Replies

1,142 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The i.MX USB Loader  is intended  for USB, not UART

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,142 Views
ko-hey
Senior Contributor II

Hi Yuri

I'm checking a following page.

GitHub - boundarydevices/imx_usb_loader: Usb loader for imx51/53/6x

I got a following description. So I guess it can download from UART.

Am I wrong ?

-----------------------------------------------

This utility allows to download and execute code on Freescale i.MX5/i.MX6 and Vybrid SoCs through the Serial Download Protocol (SDP). Depending on the board, there is usually some kind of recovery button to bring the SoC into serial download boot mode, check documentation of your hardware.

The utility support USB and UART as serial link.

-----------------------------------------------

Ko-hey

0 Kudos

1,142 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The MX usb loader uses UART/USB converter to work with UART ports of i.MX.

This may provide some problems, in particular "the UART link [host side - Yuri] uses
hardware flow control using RTS/CTS, so make sure those are available
".

Please check if the converter provides the needed settings for i.MX6 UL UART, as shown

in Table 8-39 (UART Configuration Details) of i.MX6 UL RM (IMX6ULRM, Rev. 1, 04/2016)

Regards,

Yuri.

0 Kudos

1,142 Views
ko-hey
Senior Contributor II

Hi Yuri

I'll ask them to check it.

Ko-hey

0 Kudos