Detected HDMI controller 0x0:0x0:0x0:0x0 with chip part number of MCIMX6Q4AVT10A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Detected HDMI controller 0x0:0x0:0x0:0x0 with chip part number of MCIMX6Q4AVT10A

677 Views
zhshuangp
Contributor II

Hi, all

when debug HDMI in IMX6Q, I found that "Detected HDMI controller 0x0:0x0:0x0:0x0",

based on the question link as follows,

hdmi controller 0x0:0x0:0x0:0x0

it seems that if the part number of imx6 chip is MCIMX6Q4AVT10A*, the hdmi controller is not usable ?

is it right ? can any one help to double check ?

Labels (1)
0 Kudos
3 Replies

533 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems that 3.0.35 version bsp has this issue, pls update to the latest bsp version.

0 Kudos

533 Views
zhshuangp
Contributor II

Hi Guanqiong,

The version of BSP is 3.10.17, not 3.0.35. I will try to update it to  the latest one and try again.

BTW, based on my understanding, the hdmi controller identify reg should be read as long as the module is power up normally, even if the I2C for edid is not ready ?

is it right ? any other necessary conditions if we just want to get the correct identify reg ?

0 Kudos

533 Views
joanxie
NXP TechSupport
NXP TechSupport

double confirmed from factory, "4" stands for automotive without vpu , supports hdmi too.

0 Kudos