I am using KEA8 controller. I received CW 10.5 software but it dont have KEA8 controller libraries. On site it is given CodeWarrier 10.6 need to use but I dont get link to download it.
Hello Shishir
KEA family is supported from CodeWarrior v10.6.
The latest version is v10.6.6.
Please first install CW10.6.4 which can be downloaded from:
Its update v10.6.5 and v10.6.6 are also available at the same link.
Further information and the release notes are available on the following Freescale community page:
https://community.freescale.com/docs/DOC-143655
Best Regards
Fiona Kuang
TIC - Technical Information Center
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------