Hello,
My first question Send and receive CAN frames on i.MX6xAI CPU2
I followed MX_6DualQuad_6DualLite_SABRE_Auto_CPU2_Yocto_Project_Patch_Release_Notes.pdf
i met some problem but i try build more and it built done but when i push image on sdcard and run board, run example in SocketCAN - Wikipedia, the free encyclopedia
and i can't see any signal output. Could you help me? or show me version of Linux Binary Demo Files for me can run SocketCan on board.
Any help would be greatly appreciated.
Hi manh
i.MX6 BSP supports only generic CAN APIs and unfortunately SocketCan
is not supported. One can apply to mss or nxp software partners for developing
full ready solution.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------