Dear all,
I been trying to debug my code from CodeWarrior Development 10.6 through the PnE USB multilink device but it always pop out the following messages,
I am currently using the chip processor of MC9RS08KB12.
My debug configurations:
Hope to hear from you guys soon. I really need help urgently.
Thank you. appreciate your feedback .
Hello Joonisn,
Does this can help you ? Problem with Multilink Rev C - not running after MCU V10.6 Update3 installed & CW for MCF V7.2
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Alice,
Thanks for your info. I already updated the CW software n USB multilink version. And, i had connected all pins of the flatband cable to the BDM port of my board.
But, now there is another issue on the debugging loading time. It keep showing "Downloading 312 bytes (99%)....." without completing it. Its take up the times much more longer than the usual debugging.
Do you have any idea on this ?
cheers.
Hello Joonisn,
Does the board is customer board or demo board ?
And could you please test one simple project ?
Hope it helps
Alice