I use linux3.10 and qt5 on IMX6Q, build it on yocto.the bitbake commond is as:
MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11 -e x11
bitbake fsl-image-qt5
I run the image and rootfs on my IMX6Q board, when the kernel is starting , I can see the display device( use lvds1 interface)show the yocto logo picture ,but,after the kernel starting process is finished, the display device does not show anything(the kernel running normally).What is the problem? Can you help me?
Hi jiongzhong
reason may be that lcd is not configured properly in linux,
please look at example
https://community.freescale.com/thread/355690
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------