KW40Z BLE's GAP layer defines the Central and Peripheral two roles.
I have seen examples of KW40Z_Connectivity_Software_1.0.1
( Heart Rate Sensor, Blood Pressure Sensor ...).
KW40Z only as [Peripheral] role, which is not [Central] scanning function.
To ask, to make use KW40Z [Central] function as scanning, if there is this feature and example?
What is recommended?
Solved! Go to Solution.
There are some demos in the stack that acts as a Central device in the KW40Z_Connectivity_Software_1.0.1. Some examples are:
1. hid_host
2. temperature_collector
Moreover, there is a wireless_uart_demo which could be peripheral or central. Please, see the document BLEDAUG.pdf included in the KW40Z_Connectivity_Software_1.0.1(it should be in the path: KW40Z_Connectivity_Software_1.0.1\ConnSw\doc) to have more information about how the applications work and how to play with them.
Hi Daniel,
As my friend Miguel mentioned we have some examples in our KW40 SW package , in addition pelase refer to the following post to see how to Create a Custom Profile Client & Server:
How to create a Custom Profile - Client
How to create a Custom Profile-Server
Cheers,
Antonio
Dear Antonio:
thank you
Daniel
There are some demos in the stack that acts as a Central device in the KW40Z_Connectivity_Software_1.0.1. Some examples are:
1. hid_host
2. temperature_collector
Moreover, there is a wireless_uart_demo which could be peripheral or central. Please, see the document BLEDAUG.pdf included in the KW40Z_Connectivity_Software_1.0.1(it should be in the path: KW40Z_Connectivity_Software_1.0.1\ConnSw\doc) to have more information about how the applications work and how to play with them.
Dear Jose:
Thanks.