Install Linphone apk application on mx6q and question about VP8 encode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Install Linphone apk application on mx6q and question about VP8 encode

568 Views
berniechen
Contributor II

Hi

I have got this information about VP8 "encode" is not supported for VPU

   https://community.freescale.com/thread/320030

and I verify this answer with document by following

   http://hands.com/~lkcl/eoma/iMX6/VPU_API_RM_L3.0.35_1.1.0.pdf

We installed Linphone apk, there are two options of setting for codec,1 for VP8 and 2 for H.264, I just want to know  Linphone implements this encode  technology in hardware codec or in software? If it does this implementation in hardware, is there no effective ?

Am I correct ?    Thank you.

Labels (2)
0 Kudos
1 Reply

434 Views
SergioSolis
NXP Employee
NXP Employee

Correct, VP8 is not supported by the VPU. I haven't used Linphone before, but it will be deffinitely better if its done by hardware.

0 Kudos