hello,
Using a USB3300 trying to use ulpi hs mode,
MQX 3.8 that supports external ulpi hs?
If that support is apon the MQX need to upgrade?
The purpose is created using the USB3300 NAND flash and SD card as a mass storage device
NAND Flash and SD card both want to look in the window
In that setting, where you want to use an external ulpi?
Different questions
OTG is that the HOST, DEVICE both support?
When connected to a Windows USB3300 alone device name is what?
Hi Soledad,
Thank you for answer.
This series is k60fn120 be upgraded to MQX 4.2
It does not support?
Thank you...
Hi,
MQX 4.2 supports the K60 devices however MQX 4.2 contains two USB stacks.
New USB Unified stack is designed to replace the legacy USB stack in MQX RTOS, it has an OSA layer so that it can support different operating systems, like MQX RTOS, bare metal or other RTOS (like, FreeRTOS or μCos in KPSDK).
The New USB Unified stack (usb_v2) doesn't support the k60fn120 device. The legacy USB stack supports the K60 devices, however you can port the legacy USB stack to USB_v2, please find more information about the difference between old USB stack in MQX™ RTOS and new USB Unified stack and how to port the USB unified Stack to a new platform, in the docs attached.
Regards
Sol
Hi,
MQX 3.8 doesn't support USB OTG.
For ulpi hs please check the below thread:
Virtual Communication (COM) Demo - CDC device is necessary
I hope this helps, have a nice day!
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Soledad,
Thank you for answer.
What MQX version supported?
Thank you.
Hello,
MQX 4.2 contains a new Host and Device USB stack version 2 (same as in KSDK 1.2.0).
The new USB stack is available for following platforms : FRDM-K64F, FRDM-K22F, TWR-K21F120M, TWRK22F120M,
TWR-K64F120M, TWR-K65F180M, TWR-VF65GS10, SVF522R EVB.
and below are the new added features:
Device:
Host:
OTG:
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------