SPI freezes on iMX6SL after short write and long read

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI freezes on iMX6SL after short write and long read

Jump to solution
895 Views
samuelrythm
Contributor I

Hi all,

Our custom platform based on iMX6SL meets troubles with SPI transactions. Actually it freezes in special scenario whereas it works very well otherwise.

Our environment is :

- Custom board with iMX6SL

- Linux based on FSL BSP 3.14.28

- Dev based on spidev

Our SPI is working with following scenarii, at any frequencies from 4 to 12MHz, on multiple endurance tests:

- Loop of transactions consisting in writing 1 Byte then reading 14 Bytes

- Loop of transactions consisting in reading 20x14 Bytes

Our SPI driver freezes after few transactions when :

- Loop of transactions consisting in writing 1 Byte then reading 20x14 Bytes

We observed that :

- Setting SPI bus frequency @ 12MHz seems to make it work, but it still freezes @ 10MHz / 8MHz / 6MHz / 4MHz

- Reducing the datasize to 15x14 makes it freeze in less than 1 minute

When it freezes, application cannot be killed manually, only way to get hand on SPI again is to reboot the board.

Is there any known issue on SPI driver with the couple iMX6SL <--> BSP 3.14.28?

Is there any maximum size for packet transactions?

Why writing 1 Byte before reading 20x14 Bytes makes SPI freeze whereas only reading 20x14 Bytes works perfectly?

Any help is welcome!

Thank you,

Samuel

Labels (2)
Tags (3)
0 Kudos
1 Solution
636 Views
igorpadykov
NXP Employee
NXP Employee

Hi Samuel

please try latest 3.14.52 BSP:

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

weird behaviour at different frequencies may be caused by

TKT238285, mentioned on :

https://community.freescale.com/message/482332#comment-482332

Software workaround integrated in Linux BSP codebase starting in release

imx_3.14.38_6qp_ga.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
637 Views
igorpadykov
NXP Employee
NXP Employee

Hi Samuel

please try latest 3.14.52 BSP:

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

weird behaviour at different frequencies may be caused by

TKT238285, mentioned on :

https://community.freescale.com/message/482332#comment-482332

Software workaround integrated in Linux BSP codebase starting in release

imx_3.14.38_6qp_ga.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

636 Views
samuelrythm
Contributor I

Hi Igor,

Sorry for being so long to answer but upgrading kernel was not so straightforward. We needed to include custom patches from our legacy as well.

Finally, it seems to have fixed part of the problem. Before, SPI froze systematically on large transaction TX+RX. Now it works well on endurance tests but sometimes we still meet this SPI freezing, then the kernel seems stucked, we cannot kill our application at all. So I feel like it still come from kernel space and from our user code.

To sum up, it is much better but bug still appears sometimes and is hard to reproduce...

Any other lead?

Thanks again,

Samuel

0 Kudos