i.MX6Q Slip mode(LVDS) and HDMI mirror display ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q Slip mode(LVDS) and HDMI mirror display ?

1,077 Views
yoshihikoyatsuk
Contributor I

Dear sir,

Using this i.MX6Q device , Slip mode (LVDS) and HDMI of mirror display or is possible ??

This is very difficult problem.

LVDS= 1920x1080,  HDMI=1920x1080, OS: Yocto project

Y.Yatsukura

Labels (1)
0 Kudos
3 Replies

514 Views
yoshihikoyatsuk
Contributor I

Dear Igorpadykov

I'm sorry. "Slip " instead, is the "Split" is correct.

I use 1920x1080(2 port LVDS) Panel LCD.

Thanks.

Best regards

Y.Yatsukura

0 Kudos

514 Views
igorpadykov
NXP Employee
NXP Employee

it may be useful to look at L3.10.31_dual_channel_lvds.patch.zip

https://community.freescale.com/message/525359#525359

~igor

0 Kudos

514 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yatsukura

what do you mean by "slip" ? Some mirror examples can be found on

https://community.freescale.com/thread/313507

Re: Dual Display setup on Yocto build

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos