Hi All,
Is it possible to run the Linux driver "remoteproc" on iMX6Q SabreSD board?
I want Linux to run on cores0,1 and 2 while core 3 is dedicated to an RTOS.
The latest Freescale kernel linux-imx does provide Remoteproc as a module and a modified Rpmsg.
In chapter 53, in the Linux reference manual there is a brief description on how to use RPmsg for i.MX7 and i.MX6SoloX but nothing about i.MX6Q.
Is there a similar example for i.MX6Q? If not can you please give me some guide to port the existing code from i.MX7 to i.MX6Q?
Thanks,
Tarek
Hi Tarek
unfortunately AMP is not supported for i.MX6DQ/SDL on official BSPs, one can look at
Boot The i.mx6 dual With Linux+uC/OS-II AMP
http://community.arm.com/message/15766
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------