I would like the LAY-27962_C.brd file in ASCII (ALG) or already imported into Altium Designer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I would like the LAY-27962_C.brd file in ASCII (ALG) or already imported into Altium Designer

Jump to solution
1,616 Views
bobfish
Contributor I

I am just starting a custom board using the iMX6S processor. I have the MX6SoloX SABRESDB_DESIGNFILES which contain an OrCad Schematic and an Allegro board file.

Unfortunately My company uses Altium for PCB designs. Altium will not import an Allegro board (.brd) file unless you have allegro installed on your machine, Which I do not.

I do have Capture (OrCAD) however, it would be a big time saver to have a board layout file in the ascii format which I am told can be imported into Altium.

Although we are going to modify the circuit for our application much of the processor/ memory layout would be close therefor very helpfull.

So if anyone can do the conversion or already has a converted file it would be an extremely helpful timesaver / confidence builder to have that as a starting point.

Regards,

Bob Fish

bobf@omnica.com

Labels (2)
0 Kudos
1 Solution
1,089 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bob

please look at files on

https://community.freescale.com/thread/355392

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
1,090 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bob

please look at files on

https://community.freescale.com/thread/355392

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,069 Views
nxf65583
NXP Employee
NXP Employee

Hi Igor.

I am not able to open the link you provided https://community.freescale.com/thread/355392.\

Can you please update the link. 

 

Thanking you

0 Kudos
1,089 Views
bobfish
Contributor I

This was a great help.

Thanks

0 Kudos