How do you switch a project from compiling linked KSDK source to precompiled libraries?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do you switch a project from compiling linked KSDK source to precompiled libraries?

751 Views
dave408
Senior Contributor II

I'd like to get away from having the KSDK source files linked to my project.  Ideally, I would precompile all of the KSDK libraries and then just add them to my project's linker's miscellaneous files.

So far, I believe I need, and therefore have precompiled the following:

  • ksdk_platform_lib
  • ksdk_startup_lib
  • ksdk_hal_lib
  • lib_mqx
  • ksdk_mqx_lib

I then added references to the files in my linker settings like so:

pastedImage_1.png

I think I'm really close.  Unfortunately, at the moment I get one undefined reference to DbgConsole_Init().  I am unable to delete or disable this component without PEx getting really upset with me.  I have been unable to find the location of DbgConsole_Init in any of the libraries.  All I can think of at the moment is that I need to add a link to  /platform/utilities to pull in fsl_debug_console, but wanted to see if anyone here had the same question and conclusion as me.

0 Kudos
4 Replies

535 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello dave,

Please try to build the lib of "mqx_stdlib" , then have a test.

it at here : Freescale\KSDK_1.3.0\rtos\mqx\mqx_stdlib\build\kds

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

535 Views
dave408
Senior Contributor II

Hi Alice, unfortunately, adding that library did not help.  It actually seems to not be necessary.  I get the same error with or without it added to the list of libs.

If I import the /platform/utilities folder to my project as a virtual folder, then I can make the DgbConsole_Init() undefined reference go away and the project builds.  However, at the moment it doesn't run properly, which is another topic for discussion at a later time.

0 Kudos

535 Views
vfilip
NXP Employee
NXP Employee

Hi,

this link desbribes using KSDK lib. modes in PEx project:

KSDK Library mode

best regards

Vojtech Filip

0 Kudos

535 Views
dave408
Senior Contributor II

Thanks, Alice!  I've added the extra projects to my workspace and I should have an idea soon of whether or not that was the missing link!

0 Kudos